Post Go back to editing

ADuM5241 alternatives

Hi all,

I would need a two channel isolator with just one side supplied ( Iso power, I guess) to isolate an UART.

I don't require to power anything, just to supply from one side.

My first idea was to use ADuM5241, because it has ervrything I need in a SOIC-8 (space is also important).

However, after reading bkennedy i got to the conclusion that the 5241 is an old design with too much power consumption (>80mA !)

and i guess that a part of this excess power just gonna generate EMC emissions.

A suggested replacement is the ADuM5201. Is there any other alternative with an smaller package ?

Thank you!

BBRR

JC 

Parents Reply Children