Post Go back to editing

can ADuM5230 be used to drive IGBT FS450R12OE4 ?

HELLO,

  I  want to use ADUM5230 IN  AC inverter for motor driving. Power stage is IGBT FS450R12OE4. QG=3.30uC @VGE=-15V…+15V,Cies=28.0nF,Cres=1.55nF, f=10kHz。

RGint=1.7Ω  IC nom = 450A。

  My question is : use the buffer configuration in Figure 25 in datasheet to drive this IGBT, is there anything wrong?