RS485/ RS422 3.3V device that interface to 5V device

Hi,

In my costume electronic card I have a half-duplex, ~12Mbps, RS485/RS422 Transceivers, LTC2862-1 device with 3.3Vbus. Now I want to connect to another, external LTC2862-2 device with 5Vbus (with max baud rate of ~115200bps which is O.K for both devices).

My question is that: Is it possible to connect those two devices without enable any self-protection mechanism of ether devices- in order to maintain the max devices ratability? (3.3V Vbus device that interface with 5V Vbus device and high baud rate device that interface with limited baud rate device)

Thanks,

Idan

Parents
  • 0
    •  Analog Employees 
    on Jan 29, 2019 10:30 AM

    Hi Idan,

    Both the LTC2862-1 and LTC2862-2 have a receiver up that receive data at up to 20Mbps. Your application should work without issue, the LTC2862-2 will be able to receive the 12Mbps data from the LTC2862-1, and transmit 115200bps data back.

    Both the transmitter and receiver have a wide common mode range of +25V to -25V, so there will be no issue connecting a 3.3V device to a 5V device, once you have terminated the bus.

    Regards,

    Neil

Reply
  • 0
    •  Analog Employees 
    on Jan 29, 2019 10:30 AM

    Hi Idan,

    Both the LTC2862-1 and LTC2862-2 have a receiver up that receive data at up to 20Mbps. Your application should work without issue, the LTC2862-2 will be able to receive the 12Mbps data from the LTC2862-1, and transmit 115200bps data back.

    Both the transmitter and receiver have a wide common mode range of +25V to -25V, so there will be no issue connecting a 3.3V device to a 5V device, once you have terminated the bus.

    Regards,

    Neil

Children