LTC1685
Production
The LTC1685 is a high speed, precision delay RS485 transceiver that can operate at data rates as high as 52Mbps. The device also meets the requirements...
Datasheet
LTC1685 on Analog.com
Hi!
The LTC1685 RS485 transceiver have fail-safe feature according do the datasheet.
According to your application note AN-960, the fail-safe mode is working because -30mV or more is detected as 1. and less then -0.2V is detected as 0. (However, the threshold voltages for LTC1685 according to datasheet is less than -0.3V is 0 and more than 0.3V is 1.)
Assuming the same is true for LTC1685, that -30mV or more is 1 it works without any external bias of the A and B inputs.
If we want to increase the noise margin, a small external bias should be applied to the A and B inputs. This is done in the datasheet in Figure 15. However, the bias seems to be in "wrong" direction. The B input is driven high and the A input is driven low. Why is it like this? Should not the A input be driven to the positive supply and the B input driven to ground as shown in Figure 9 in AN-960?
Best regards
Joakim
Hi Joakim,
For RS-485 in general, the supply biasing is on the A wire and the ground biasing is on the B wire, per AN-960.
After reviewing LTC1685 datasheet, the diagram you referred to specifically shows biasing in a particular application that was relevant at the time the part was released. The SCSI protocol apparently uses a termination and biasing network per the diagram - i.e. 330 Ohm to supply on the "-" wire and 330 Ohm to ground on the "+" wire, with 150 Ohm in between. I'm not familiar with the reasons for this approach, but it is particular to this standard.
There are other standards too that dictate particular termination networks, e.g. Profibus, but typically these have supply biasing on the non-inverting signal (A or "+").
Regards,
Conal