Post Go back to editing

LTC1685 IBIS model

Thread Summary

The user inquires about implementing a series resistor on the RO output signal for the LTC1685 transceiver to ensure good signal integrity with 50Ω transmission lines. The support engineer confirms that no IBIS model is available for the LTC1685 but provides an estimate of the output impedance using the VOH specification: (5.0 V - 4.8 V) / 4mA = 50 ohm.
AI Generated Content

Hi!

I like to implement a serie resistor on RO output signal (pin 1) when using 50R transmission lines for good signal integrity. Hence the following questions:

1. Is there any IBIS model available to the LTC1685 transceiver?

2. What is the approximate output impedance of the RO output signal?

Best regards

Joakim

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.