Article Can I use the MAX3421E with any microcontroller?

As long as a microcontroller has SPI capabilities, via an SPI peripheral or through a bit-banged GPIO interface, it should be able to work with the MAX3421E. The SPI interface on the MAX3421E is referenced to a user-supplied VL logic rail. Please ensure the logic voltage for the microcontroller matches the voltage applied to VL.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.