Article The MAX1481 datasheet (Rev 1 3/06) states that “The receiver input has a failsafe feature that guarantees a logic-high output if the input is open circuit.” However, the EC table also specifies Receiver Differential Threshold voltage as +/-200mV. Do these

The two descriptions do not contradict each other. MAX1481 has a failsafe feature where there is a weak pullup to VCC at input A and a weak pulldown at input B. When input is open, input A is pulled up and input B is pulled down, pulling differential voltage across A and B to be above 200mV, and ensures that RO outputs a logic-high. However, since the internal pullup and pulldown are both very weak, any external connection will override the internal pullup and pulldown. It only maintains a logic-high under open circuit condition, and does not conflict with the input threshold.
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.