Article How to use RESET pin of MAX22513

Question:

RESET pin of MAX22513 has dual function of reset input and POK output. How should we use this pin?

Answer:

The new RESET Pin has the following functions

>Power OK Function

•RESET/POK is an open-drain logic output/input that needs a pull-up resistor to VL or VCCB to operate as POK

•RESET/POK is low when the DC/DC and V5 supplies are low

>Note that the VL supply must be present for MAX22513 to be able to actively pull RESET/POK low

•RESET/POK goes high with a delay of 3.3ms/4.4ms after the DC/DC and V5 are in normal operating range 95% of set DC/DC voltage)

>RESET Function

•RESET/POK is also a (active low) RESET input

•When RESET/POK is pulled low, the Registers are reset to default value

•When RESET/POK is driven low, the C/Q and DO drivers are tri-stated

•When RESET/POK is high, both drivers will be operational

>If the DC/DC is not used, then the FB pin must be connected to VCC, so the chip thinks the DC/DC power is OK

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.