Article The D+ D- signal during USB operation of the MAX3420 looks very strange, but USB functions and the system passes compliance testing. How is this possible?

Many engineers have noticed that USB full speed signals appear very strange when probed with an oscilloscope. The transmitted waveform seems to have a “shelf” at about ½ the signal amplitude.  This shelf is normal and is expected. What you see on the USB D+ or D- signal lines during USB traffic in a full speed environment is due to the transmission lines being terminated in the characteristic impedance on only the transmitting end of the cable. This “shelf” at ½ of the signal amplitude is the time it takes for the signal edge to propagate past the point of the probe and then reflect back from the un-terminated receiver end of the USB cable.  With long 5 meter USB cables, the “shelf” or stair step in the signal can be very long in time and makes the signal appear distorted. With a short USB cable ( ~ 6 inches) it may not be possible to observe the “shelf” in the waveform due to the short time delay of the cable relative to the pulse rise and fall times for a USB full speed signal.

One other aspect of the USB signal is that it is differential, and probing in a single ended fashion can also be misleading about the true nature of the signal.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.