Article What is the purpose of the 1k ,10k and zener in the application circuit of MAX77301?

 
 

The resistor-diode network is a proposed workaround for BATT to BUS leakage problem. The reason for the 1k,10k resistors  is as follows:

The control circuit which shuts off the current path from Bat to Bus does not operate when Int_3V3 is lower than 80% of the Bus voltage. The added 11K resistance between INT3v3 and BUS helps prevent INT3v3 discharge faster than BUS when charger disconnect, thus preventing the possible Bat to Bus leakage issue.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.