Article ADuM5401: How do I connect PIN 7 (RCout) of ADuM5401 in a standalone application?

Question

How do I connect PIN 7 (RCout) of ADuM5401 in a standalone application?
To Vdd1 or not connected ?

Answer

The RCout pin should be left as a no connect unless it is being sent to an RCin
pin of an ADuM520x or ADuM5000.
(RCout is Regulation Control Output. This pin is connected to the RCIN pin of a
slave isoPower device to allow the ADuM5401 to control the regulation of the
slave device).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.