Article Is ADuM6000 (or ADuM5000) compliant with the USB low power suspend mode current limits?

Question

Is ADuM6000 (or ADuM5000)compliant with the low power “suspend mode” as defined
for USB 2.0/3.0 (2.5mA limit in low power suspend mode).

Answer

There is no support for USB suspend mode in the ADuM6000. The ADuM5000 and
ADuM6000 can be suspended to draw very little current, <
the secondary side and resuming would be an issue. There would also need to be
some processor control to suspend the part from the Upstream side. Whether
this would be useful depends on the details of the particular application.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.