Article ADuM6400: PCN # 11-0188 typo error

Question

PCN # 11-0188 for the ADuM6400 states that the maximum current has been changed
from 500mA to
400mA. I can find no reference to a maximum current of 500mA in the Rev. 0
data sheet?

Answer

The PCN # 11-0188 has a typo, there should be a correction posted shortly for
this PCN
The ADuM6400 part is changing from 500mW to 400mW maximum output power. This
is the rating
for 5V/5V operation. The current in that condition is changing from 100mA to
80mA. This is due to
thicker polyimide between the power transformer coils.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.