The clock signal is required when the MAX9271 and similar serializers transmit data and commands. To overcome issues such as the absence of the video signal, thereby missing the pixel clock ( PCLK ), the…
The MAX9271 can be used with the MAX96706.
The MAX96705 can also be used with the MAX96706. The difference between the MAX9271 and MAX96705 is that the MAX9271 does not have HIM (High-Immunity/Bandwidth…
The MAX9271/2 transmits in units of frame . To eliminate the DC component during transmission, a 8b/10b encoding is performed prior to transmission. As such, the 24 -bit and 32 -bit data are encoded into…
The outside of the coaxial cable is a shield layer. The signal is transmitted in the center conductor and the inner surface of the shield layer. EMI radiation to the outside is minimal. It is also difficult…
ADDx , CX/TP , I2CSEL , SD , HIM and BWS pins are latched after leaving the Power-Down Mode. Then the voltage level at the pins will not effect the corresponding functions of the pins. However, the MS…
MAX9271 transmits data with frames as a single unit. Each frame includes 24 bits or 32 bits of data. As shown in the following: In regards to applications for the camera, since most camera outputs in Raw…