Article MAX77757 CHGIN BYP pins voltage relationship

Question

What will the voltage be on BYP pin of the MAX77757 if Vusb/Vadp is higher than 5.1V (9V for example)? Would it be the voltage replica of the input voltage? Or would it be the voltage bucked by Qchgin?

 

Answer

The BYP and VUSB nodes are separated for input current sensing and controlling the switch for OTG (USB On the Go) support. The BYP is the switching node input, so it has the input capacitance. The voltage at CHGIN is the same as BYP. The voltage step-down happens between the BYP the SYS nodes.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.