MAX14934: FAQ

  • How much current can the digital isolator MAX14934 source/sink?

    All outputs on the MAX14934 have a push-pull output structure. The recommended source/sink current is 4mA, which will yield at most a 0.4V difference from VCC when sourcing and 0.4V difference from GND…
  • MAX14934/5/6 Leakage Current

    Q: How much leakage current can I expect across the isolation barrier of the MAX14934? A: We don't spec a maximum for the leakage current, but it can be easily calculated based on the given impedance…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.