Article What is the correct configuration for DI/TTLY, DI/TTL2, and DI/TTL3 to ensure proper operation in D-HTL mode on MAX14890E in pin control mode?

 
Answer:
 
In pin-control mode, users must set the SNGL/CLK and TTL/SDI inputs low to enable D-HTL functionality for the RxA, RxB, and RxZ receivers. DI/TTLY, DI/TTL2, DI/TTL3 are not used in D-HTL mode and do not affect it. They are only used to select DI/TTL on RxY, RxD2 and RxD3 when SNGL/CLK is L and TTL/SDI is L. RxY, RxD2 and RxD3 can never operate as D-HTL receivers. This can be seen in the truth tables on the MAX14890E datasheet.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.