Article Should I add TVS didoes at the input pins of the MAX14890E?

Yes, TVS protection is generally needed against ESD and surge, since the part does not have inside.  Which TVS depends on the application requirements.  Some DI/DO applications require 2kV/42Ohms, which translates to 42A of peak surge current for example  The requirement may be lower for data interfaces.   
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.