Article Is the MAX14827 capable of detecting wakeup events when the C/Q pin is configured as input?

No, the MAX14827 is only capable of wakeup events when the C/Q pin is configured as an output and the C/Q driver is enabled.  For a wake-up to occur, the C/Q line must be in push-pull, high-side (PNP), or low-side (NPN) modes.  These operation modes only occur when the C/Q is an output.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.