Article What is the Difference between MAX14827 and MAX14827A?

The only difference is that the MAX14827A device improved ESD rating is 2kV while the non "A" version MAX14827 ESD rating is 1kV.

At this point Maxim continues to sell both versions.  This is because of existing customers already having qualified the MAX14827 in their design may not want to go through a re-qualification to change the part number to MAX14827A.
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.