The MAX14783E is designed to withstand ±35kV ESD HBM, but surge protection at 2kV/4kV levels requires additional protection on the bus lines.
Customers will need to add external protection to be able…
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the