ADUM4160/ADUM3160: Can these devices support OTG (On The Go) USB?

  • Created
  • Updated
Was this helpful?
  • ADuM4160 PIN input

    Question We are using ADuM4160 in an ECG module. What voltage is required at PIN input to activate the pull-up resistor ? Answer The PIN input like all of the control lines is a 3.3V digital input so…
  • ADuM4160 wiring with uC

    Question In a current design of a medical device, i have to establish an isolated USB connection between a PIC microcontroller and a host and I intend to use the ADuM4160 for that purpose. My microcontroller…
  • ADuM4160 with SMSC USB2514B

    Question We want to use ADuM4160 in an isolated USB HUB but have the following problem: we need to isolate only 2 USB ports of SMSC USB2514B USB Hub (attached). However, USB line pairs USBDNx-Dx from…
  • ADuM4169: Powering VBUS1 from 5V and VBUS2 from 3.3V.

    Question I am looking at using the ADUM4160 USB Digital Isolator powering the input VBUS1 side from the 5V computer input but the VBUS2 side from 3V3. Looking at the datasheet it would appear that…
  • EVAL-ADUM4160 physical dimensions

    Question I have the User Guide for this evaluation board but can you tell me the physical dimensions and mounting hole spacing please. I want to use a number of them in some items of custom functional…
  • Pull-Ups on SPU and SPD

    Question A board we are producing that uses the ADuM4160 fails during production test. When comparing the design with an article in Analog Dialog 43-06, june 2009 I noticed that the design of our customer…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.