Q
What does the 1% accuracy of the ADuM3190/4190 include?
A
The 1% accuracy specification includes the use of the ADuM3190/4190 in an
isolated feedback loop and includes drift over temperature from -40˚C to 125˚C.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the