ADUM3160/4160: Can this device be used for USB-IF standard host isolation

  • Created
  • Updated
Was this helpful?
  • ADuM3160 for USB isolation

    Question I want to use the ADUM3160 to isolate a USB Line. The ADUM3160 must be connected direclty to a PC USB output, and have to drive a USB cable and the USB peripheral. What I want to know is,…
  • ADuM3160 USB speed and compatibility

    Question I am currently working on a design which integrates an isolated USB-Hub. For the isolating, I am planing to use the ADuM3160BRWZ. But now I am completely confused about the USB speed and compatibility…
  • ADuM3160 with USB2.0 & 3.0

    Question I have a device in production where I use the ADUM3160 to isolate an USB HID pheripheral. I never face any problem till now. In some PC with a USB3.0 (RENESAS USB 3.0 HOST CONTROLLER) the…
  • ADuM3160_USB OTG

    Question We are using ADUM3160 in our products where we need USB port isolation , and it is working nicely . However , so far , all our applications involved our product being the ‘device’ , i.e. it…
  • ADUM4160/ADUM3160: What is the difference between these 2 USB isolation devices?

    Question What is the difference between the 2 USB isolation devices, ADUM4160/ADUM3160 Answer There are two differences, insulation rating and operating power supply range. ADUM3160: Insulation Rating…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.