ADUM3070: FAQ

  • ADUM3070 Creepage and Air Clearance specifications

    Q What are the specification for creepage distance and air clearance for ADUM3070? Datasheet states minimum spec; what are the actual values? A The creepage of the ADuM3070 QSOP package is on average…
  • ADuM4070 with high input voltage and 3.3V 1A output

    Question 1. I have already used the AduM3070, as isolated Power supply of 2W. Now I would use this chip to make an isolated power supply of 3.5W-4W, as I need to solve space. Do you have any application…
  • Common-Mode voltages on ADuM3070 / ADuM4070

    Question We're making a test board for a very noise sensitive sensor. It has to be galvanic isolted so we want to use the AdUM3070 or AdUM4070 for this. What is the difference between these two? After…
  • Power calculation for ADuM3070

    Question Attached you can see a block diagram of our power design. Is the ADuM3070 / 4070 able to deliever enough power for this design in the 5V -> 5V configuration? Total power on the galvanic isolated…
  • RE: Split Isolated Supply with isoPower query(SR#: 1204350)

    Q Is it possible to create a split isolated supply with the isoPower devices (i.e. ±3.3V or ±5V). A This can be done one of two ways. 1) Use the ADuM347x or ADuM3070. These devices use external…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.