Question we would like to use Your “Digital Isolators” (ADuM...) in our applications.
But we have an operating input/output-voltage difference of more than 2KV,
which is not supported by the “Digital…
Question Problem description:
I have found that narrow pulses of about 5ns cause the output to respond to
only one edge and produce a pulse of many hundreds of nanoseconds until the low
frequency…
Question We are using ADuM1250 for I2C isolation in our product (for industrial
automation). Side 1 is supplied by VDD1=3.3V and SCL1 and SDA1 are pulled up to
the same VDD1=3.3V. Side 2 of the isolator…
Question My customer have a failure issue with ADuM1250ARZ - Hot Swappable, Dual I2C
Isolators
Please see follow his description:
Until now we already assembled about 100 components, on 3 of them…
Question I want to know if it is possible to connect a I2C device to the Side 1 of your
ADuM1250 chip. The I2C device has SDA,SCL Input Logic-High (Vih) of 1.4 V
minimum, SDA,SCL Input Logic-Low (Vil…
Question I want to use the ADUM1250/51 in a battery application. Are there some
tips to decrease the power in this type of application? Answer The ADuM1250 consumes a certain amount of power when idle…
Question I am getting a little confused. What is the maximum permited voltage under IEC
61010 for reinforced insulation using this part? Answer The ADuM2251 is the 5 kV version of that part (ADuM125x…
Question I am using ADuM1251 to cross the safety boundary mains input to touchable
output in a switch mode power supply. As part of testing the following test
voltages are applied:
1.5Kv AC 2Kv Dc…
Question I have a customer using ADuM1251 for their I2C isolation application.
But currently, they meet the below picture status (Figure 1):
Figure 1
This is tested from our ADuM1251 primary…
Question I am using ADUM1301; could you please provide me the output current capability
(sourcing the current) for the pins 13(VOB) and 14(VOA). Answer Page 4 of the ADuM1301 datasheet states that the…