ADM3053: FAQ

  • ADM3053 max current on Visoout

    Question What max current can be drawn on the Visoout (PIN 12).We need to drive a external low voltage LED on the CAN-Bus side. Answer Thermal considerations (power dissipated internally in the part…
  • ADM3053 Round Trip Propogation Delay

    Question Please can you tell me if the ADM3053 has a round trip propogation delay of This is a requirement I have to meet in a CAN bus Vehicle network. Answer The ADM3053 has a maximum round trip delay…
  • ADM3053 stitching capacitance

    Question I redesign a board, In that board I used the ADM3053. In previous version of this board I have problems related with EMI (the board is out of Class B Limits). I have a limited space for ADM3053…
  • CAN FD version of ADM3053

    Question Does ADI offer a higher speed- CAN FD version of ADM3053? Answer No not at present (Feb 2015), but we do plan to support CAN FD and hope to have a device to sample in 2016.
  • Propagation Delay: 4.7KOhms

    Question Could you give me the propagation delay For · Propagation Delay from TxD On to Receiver Active : "tonRxD" Rs= 4,7kOhms, · Propagation Delay from TxD Off to Receiver Inactive: "toffRxD" Rs =4,7kOhms…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.