ADM2682E: FAQ

  • ADM2682E/ADM2687E Creepage and Clearance

    Question What creepage and clearance does the ADM2682E/87E have, and what do these characteristics refer to? Answer The ADM2682E/87E has more than 8 mm of creepage and clearance. Creepage refers to…
  • ADM2682E/ADM2687E Isolation Voltage

    Question What isolation voltage does the ADM2682E/87E meet? Answer The ADM2682E/87E provides an isolation withstand voltage of 5 kVrms per UL1577 between the two sides of the isolation barrier. This…
  • ADM2682E/ADM2687E providing additional current to external devices

    Question Can the internal isolated DC/DC converter provide additional current to external devices using the Visoout pin? Answer No, the internal DC/DC converter only has sufficient power to power the…
  • ADM2682E/ADM2687E Recommended Application Notes

    Question Do you have any recommended application notes that would help design in the parts? Answer Please go to www.analog.com and search for: AN-0971: Recommendations for Control of Radiated Emissions…
  • Difference between ADM2682E and ADM2687E

    Question What are the differences between the ADM2682E and ADM2687E? Answer The only difference between the two parts is the data-rate, the ADM2682E is a 16Mbps part and the ADM2687E is a 500kbps part…
  • Key difference between the ADM268xE and ADM258xE

    Question What’s the key difference between the ADM268xE and ADM258xE? Answer The key difference is the isolation rating. The ADM268xE is a 5kVrms rating per UL1577, whereas the ADM258xE is a 2.5kVrms…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.