capture of the output
capture of the output
More interesting thing is that I can't assign the ip address by dhcp server. My dhcp/bootp server never never get a message from this evaluation board.
Hello Max,
My apologies for the delay. Do you have visual studio in place?
Please let me know.
Thanks,
No. Why do I need visual studio?
It is recommended as it is the source code for ni-example-app. What this ends up being is that this is a known issue with ni-example-app and the fix is a one line change in the source code. If you can't get your hands on visual studio, please let me know.
It is recommended as it is the source code for ni-example-app. What this ends up being is that this is a known issue with ni-example-app and the fix is a one line change in the source code. If you can't get your hands on visual studio, please let me know.
Hi Max,
I have created a module in SSD that corrects this issue, It is basically a 6.0.3 release that fixes the issue you are seeing.
Please send me a message with your email and I will open up the SSD module so you can continue evaluating our product.
To anyone else on this thread who wishes to solve this problem and does not have a visual studio license. Please send me a message with your email and I will add you to the SSD module as well.
Dear DET_CStelmar,
Thank you for fixing this issue. We switched this product to the AD's Fido5100 chip and will write the driver to interface to our EIP software instead. I do not have the time and urgency to keep trying this evaluation board anymore. I will do it later if necessary!
Regards,
Max