capture of the output
More interesting thing is that I can't assign the ip address by dhcp server. My dhcp/bootp server never never get a message from this evaluation board.
Hello Max,
My apologies for the delay. Do you have visual studio in place?
Please let me know.
Thanks,
No. Why do I need visual studio?
No. Why do I need visual studio?
It is recommended as it is the source code for ni-example-app. What this ends up being is that this is a known issue with ni-example-app and the fix is a one line change in the source code. If you can't get your hands on visual studio, please let me know.
Hi Max,
I have created a module in SSD that corrects this issue, It is basically a 6.0.3 release that fixes the issue you are seeing.
Please send me a message with your email and I will open up the SSD module so you can continue evaluating our product.
To anyone else on this thread who wishes to solve this problem and does not have a visual studio license. Please send me a message with your email and I will add you to the SSD module as well.
Dear DET_CStelmar,
Thank you for fixing this issue. We switched this product to the AD's Fido5100 chip and will write the driver to interface to our EIP software instead. I do not have the time and urgency to keep trying this evaluation board anymore. I will do it later if necessary!
Regards,
Max