Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

About ADIN1300

1. Can the Generic Driver of the Linux kernel drive this chip?

2. Does the driver provided on the official website support linux3.10 kernel?

3. Can the chip be connected to EMAC?




[locked by: CatherineR at 8:35 AM (GMT -4) on 3 May 2023]
Parents
  • Hi Geoff,

    Yes the generic Linux driver can be used with the ADIN1300 as long as the only registers being used are the first 16 generic registers.

    The current Linux driver available is compatible with version 4.19 and is not backwards compatible.

    The ADIN1300 can be connected to multiple MAC interfaces such as MII, RMII and RGMII.

    Best Regards,

    Mark

Reply
  • Hi Geoff,

    Yes the generic Linux driver can be used with the ADIN1300 as long as the only registers being used are the first 16 generic registers.

    The current Linux driver available is compatible with version 4.19 and is not backwards compatible.

    The ADIN1300 can be connected to multiple MAC interfaces such as MII, RMII and RGMII.

    Best Regards,

    Mark

Children
No Data