Post Go back to editing

RPG2 (Profinet, EV-RPG2PNZ-U1) test problems

Hi there,

I got an EV-RPG2PNZ-U1 and got some problems during testing.

  1. I followed the instructions of RPG2 PROFINET Quickstart Guide/UG-1850. Used ni-example-app.exe to setup the EVB.
    After I typed ni-example-app.exe –l ETH –n {XXXXXXXX-XXXX-XXXX-XXXX-XXXXXXXXXXXX}, configuration went on but several messages of "FATAL Bad Memory Block" appeared.
    Somehow the EVB was set ready after the whole process.
    If I enter the command with addition of "\Device\NPF_", the configuration seemed failed.
    By the way, I installed the latest package of NPCap.
    And I put the error message at the bottom of this thread.
  2. Besides a Siemens PLC that the guide suggests for testing the RPG2 platform, is there any other suggestion?
    Like using other analysis or simulation software? E.g. PRONETA by Siemens (https://new.siemens.com/global/en/products/automation/industrial-communication/profinet/proneta.html)

----------

C:\Users\User>ni-example-app.exe -l ETH -n {DDB59474-6FB5-4493-AC68-9401EE59461F}
Welcome to ni-example-app!

Processing arguments...
DONE
Performing system startup...
DONE
Start time update process...
DONE
Starting up example application...
DONE
Link init...
DONE
Unified Interface stack init...
DONE
Set response timeout...
DONE
Find Network Interface...
FATAL Bad Memory Block.
DONE
Reset Network Interface...
FATAL Bad Memory Block.
DONE
Wait 10000 us for module to finish reset...
DONE
Get installed protocol...
FATAL Bad Memory Block.
DONE (PROFINET)
Set device 400...
FATAL Bad Memory Block.
DONE
Add item 500 to location 1...
FATAL Bad Memory Block.
DONE
Add item 501 to location 2...
FATAL Bad Memory Block.
DONE
Add item 502 to location 3...
FATAL Bad Memory Block.
DONE
Set transmit modes...
FATAL Bad Memory Block.
DONE
Finalize configuration...
FATAL Bad Memory Block.
DONE

----------

C:\Users\User>ni-example-app.exe -l ETH -n \Device\NPF_{DDB59474-6FB5-4493-AC68-9401EE59461F}
Welcome to ni-example-app!

Processing arguments...
DONE
Performing system startup...
DONE
Start time update process...
DONE
Starting up example application...
DONE
Link init...
Error opening source: Error opening adapter: 操作順利完成。 (0)

List of available network devices:
1: {1C5CF92E-D3E8-4F6D-8F52-DA7AC7EDEAC9}, (Microsoft)
2: {A8C6DD9D-A749-4C73-AAB8-D5D929C25ABC}, (Microsoft)
3: {24AACFD5-3977-4335-B911-7A7B23B8A884}, (Microsoft)
4: {897ADB73-EA29-4686-AB9A-AAA82103DDBC}, (Microsoft)
5: {1654ECF2-60EB-4630-BB46-1D4D0DB0626C}, (Realtek PCIe GbE Family Controller)
6: {DDB59474-6FB5-4493-AC68-9401EE59461F}, (Realtek USB NIC)

FAILED

Parents Reply Children
No Data