Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Physical Layer Devices
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Physical Layer Devices
  • Industrial Ethernet Solutions
Physical Layer Devices
Documents ADIN1300 Gigabit Ethernet PHY Bootstrapping
  • Q&A
  • Videos/Images
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADIN1300: FAQ
    • ADIN1300 Gigabit Ethernet PHY Bootstrapping
    • Are ADIN1200 and ADIN1300 supported by U-Boot?
    • ADIN1300 Exposed paddle and Keepout area
    • ADIN1300 Typical Link Times FAQ
  • How to create a 10BASE-T1L range extender?

ADIN1300 Gigabit Ethernet PHY Bootstrapping

Original Question: FAQ: ADIN1300 Gigabit Ethernet PHY Bootstrapping by CatherineR

Q: What PHY features can be bootstrapped at power up?

A: The PHYs hardware configuration pins allow users to predefine the personality of the PHY for unmanaged applications. The features that can be configured by bootstrapping are as follows:

  • PHY Address
  • Forced/Advertised mode
  • PHY Speed
  • Software Powerdown Mode after Reset
  • Downspeed Enable
  • Energy Detect Powerdown Mode
  • EEE Enable
  • Auto-MDIX
  • MAC Interface Selection (RGMII/RMII/MII)

Unmanaged configurations allow the PHY to power up in a particular condition without the need to communicate with the part over the MDIO interface. This means that a link can be brought up quite quickly after power on if there is a link partner present.

The hardware pin configurations are set using external resistors on various pins. Review the datasheet section on Hardware configuration pins for full details.

Note that some pins use 4-level strapping (Mode 1-4), whereas other pins only use two level strapping (high & low).

The PHY address pins use two level strapping.

Tags: ethernet phy phy ADIN1300 Physical Layer devices mdio Gigabit PHY PHY speed auto-MDIX Show More
  • Share
  • History
  • More