| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Missed after 81 hours |
RGrau MStokowski SMohammadi folivier |
Assigned |
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
ADIN2111
Recommended for New Designs
The ADIN2111 is a low power, 2-port 10BASE-T1L transceiver designed for industrial Ethernet applications, and is compliant with the IEEE® 802.3cg-2019â...
Datasheet
ADIN2111 on Analog.com
Hi
The EVAL-ADIN2111 has a center tap at T1, to which C98, R82, and C103 are connected. According to simulations using LTspice,
there is no difference in AC characteristics whether C98, R82, and C103 are present or not.
Are C98, R82, and C103 necessary?

MDI Components. 10BASET1L, ADIN2111, EVAL-ADIN2111D1Z, - Q&A - Physical Layer Devices - EngineerZone
NKokubo131 - Moved from Physical Layer Devices to LTspice. Post date updated from Tuesday, June 9, 2026 4:45 AM UTC to Wednesday, June 17, 2026 2:55 AM UTC to reflect the move.
NKokubo131 - Moved from Physical Layer Devices to LTspice. Post date updated from Wednesday, June 17, 2026 2:55 AM UTC to Wednesday, June 17, 2026 2:55 AM UTC to reflect the move.
MStokowski - Moved from LTspice to Physical Layer Devices. Post date updated from Tuesday, June 9, 2026 4:45 AM UTC to Thursday, June 18, 2026 6:20 PM UTC to reflect the move.
MStokowski - Moved from LTspice to Physical Layer Devices. Post date updated from Thursday, June 18, 2026 6:20 PM UTC to Thursday, June 18, 2026 6:20 PM UTC to reflect the move.
Hi NKokubo131 ,
As you have mentioned the other thread (https://ez.analog.com/industrial-ethernet/physical-layer-devices/f/q-a/593414/mdi-components-10baset1l-adin2111-eval-adin2111d1z)
C98, R82, C103 provide common-mode termination through the center tap and help to provide EMC immunity. We do recommend to keep them if you are using a transformer with a center-tap.
Kind Regards
Olivier
Hi NKokubo131 ,
As you have mentioned the other thread (https://ez.analog.com/industrial-ethernet/physical-layer-devices/f/q-a/593414/mdi-components-10baset1l-adin2111-eval-adin2111d1z)
C98, R82, C103 provide common-mode termination through the center tap and help to provide EMC immunity. We do recommend to keep them if you are using a transformer with a center-tap.
Kind Regards
Olivier
Hi
Thank you for your reply.
What problems might arise if a 350uH transformer without a center tap is used?
Best regrads
N.Kokubo
Hi NKokubo131 ,
As stated in the shared thread (https://ez.analog.com/industrial-ethernet/physical-layer-devices/f/q-a/593414/mdi-components-10baset1l-adin2111-eval-adin2111d1z),
The EVAL-ADIN2111D1Z doesn't have a transformer with a center-tap while the EVAL-ADIN2111EBZ has one, however regarding performance, both the evaluation board designs ensure compliance with the10BASE-T1L standard. The difference in components does not degrade the performance.
Kind Regards
Olivier