Post Go back to editing

When using ADIN1200 in MII mode, the clock drops from 25MHz to 2.5MHz when link down is detected.

Category: Datasheet/Specs
Product Number: ADIN1200

Regarding the ADI Ethernet transceiver (PHY) ADIN1200 (model number: ADIN1200BCP32Z),
I would like to make the following inquiry regarding the behavior of the clock output when the PHY detects a link-down.

The PHY speed setting is set to 100FD with auto-negotiation disabled.

The measured input voltage of PHY_CFG0 at startup is 2.8V.

PHY_CFG1 is 2.3V, and measurements have confirmed that both are within the MODE3 range.

When operating with the above settings, we have confirmed that the TX_CLK output drops from 25MHz to 2.5MHz within 10us of detecting a link-down.

・Question 1: Please tell me why the above behavior occurs.
I have looked at the data sheet, but I still don't understand the cause of the above behavior, so I would appreciate it if you could explain.

・Question 2: Please tell me what settings I need to make so that the 25MHz clock output continues even when the link is down.

Parents
  • Hi,
    This behavior is expected. The MII clocks are speed dependent, 25 MHz for 100BASE‑TX and 2.5 MHz for 10BASE‑T, so when the link drops the ADIN1200 keeps TX_CLK running but idles at 2.5 MHz which is 10 Mb/s timing; this occurs even when autonegotiation is disabled and 100 Mb/s full‑duplex is forced, because the standard ties the MII clock rate to the active/resolved link speed, not to a forced speed setting in link down.

    Do you require a continuous 25 MHz clock even during linkdown? If so, what uses it, and what fails when it drops to 2.5 MHz?

    regards,

    Mark

Reply
  • Hi,
    This behavior is expected. The MII clocks are speed dependent, 25 MHz for 100BASE‑TX and 2.5 MHz for 10BASE‑T, so when the link drops the ADIN1200 keeps TX_CLK running but idles at 2.5 MHz which is 10 Mb/s timing; this occurs even when autonegotiation is disabled and 100 Mb/s full‑duplex is forced, because the standard ties the MII clock rate to the active/resolved link speed, not to a forced speed setting in link down.

    Do you require a continuous 25 MHz clock even during linkdown? If so, what uses it, and what fails when it drops to 2.5 MHz?

    regards,

    Mark

Children
No Data