Post Go back to editing

Regarding connection between ADIN1100 and 100Base-Tx

Thread Summary

The user inquires about connecting an ADIN1100 (10BASE-T1L) to a 100BASE-TX. The final answer suggests using a switch or MCU for buffering, or forcing the 100BASE-TX PHY to operate at 10 Mbps, such as with the ADIN1200, to avoid overflow and packet loss.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADIN1100

I'm thinking of connecting an ADIN1100 to a 100Base-Tx.
I understand that the ADIN1100 (T1L) only supports up to 10base.
Is there any way to address this by adding buffer memory or something similar when a 100Base signal arrives?

Could you please give me some advice on connecting an ADIN1100 to a 100Base-Tx?

  • Hi  

    Thank you for reaching out to us.

    You're right, you can't connect a 100BASE-TX directly to a 10BASE-T1L PHY like the ADIN1100 without some form of buffering in between.

    You could use a switch (SES, for example) or an MCU, between the two. They will handle the bridging and buffering.  However, if the 100 Mbps side pushes too much data, the buffers can overflow leading to packet loss.

    Alternatively, you could force the 100BASE-TX PHY to run at 10Mbps instead of 100Mbps so they can be connected back to back without a switch or MCU for buffering traffic. However, you may need an MCU for configuration if needed. For example, you could use the ADIN1200 and force it to operate at 10 Mbps using an MCU.

    Kind Regards,

    Shazia

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.