I'd appreciate ADIN1101 evaluation board schematic or reference design, specifically for new hybrid implementation compared to ADIN1100
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 0 hours |
SMohammadi RGrau |
Open |
ADIN1101
Recommended for New Designs
The ADIN1101 is a low power, single port, 10BASE-T1L transceiver
designed for industrial Ethernet applications and is compliant with
the IEEE® 802.3cg...
Datasheet
ADIN1101 on Analog.com
ADIN1100
Recommended for New Designs
The ADIN1100 is a low power, single port, 10BASE-T1L transceiver designed for industrial Ethernet applications and is compliant with the IEEE® 802.3cg...
Datasheet
ADIN1100 on Analog.com
I'd appreciate ADIN1101 evaluation board schematic or reference design, specifically for new hybrid implementation compared to ADIN1100
SMohammadi - Moved from Other Products (EN) to Physical Layer Devices. Post date updated from Tuesday, July 15, 2025 12:03 AM UTC to Wednesday, July 16, 2025 8:26 AM UTC to reflect the move.
Hi AlexGZ
The EVAL-ADIN1100EBZ schematic can be used as a reference. Since the hybrid and termination resistors are internal, the only difference is in the MDI circuitry.
The MDI interface circuitry difference between the two devices is as follows:
ADIN1100:

ADIN1101:

The recommended MDI circuitry can be found in the ADIN1101 datasheet, page 16. Snapshot attached.

Kind regards,
Shazia
Thank you, Shazia!
How about interfacing ADIN1101 using RMII with 10/100 Ethernet PHY, strapping, clocking,...?
Hi DigiLab,
You can refer to the EVAL-ADIN1100EBZ board as a reference to the MII connection with the ethernet PHY. Noting that the difference between the ADIN1100 and ADIN1101 is the MDI circuitry as illustrated above.