Post Go back to editing

MDI Components. 10BASET1L, ADIN2111, EVAL-ADIN2111D1Z,

Category: Hardware
Product Number: EVAL-ADIN2111D1Z

Hello,

I've recently seen that you have release a new Evaluation Board called EVAL-ADIN2111D1Z. You also have another Eval Board (EVAL-ADIN2111EBZ).

The thing is EVAL-ADIN2111EBZ does respect the typical 10BASE-T1L MDI use of components (C98, R82, C103) but the new EVAL-ADIN2111D1Z doesn't have these components.

Do it have a specific reason? Do it affect to the performance? Which is the best solution?

Thank you,

Edit Notes

MDI, not DMI.
[edited by: inagore at 1:16 PM (GMT -4) on 10 Mar 2025]
  • Hi  

    The reason is that the new board EVAL-ADIN2111D1Z supports power forwarding. We selected a larger transformer to allow the use of smaller 47uH power coupling inductors while maintaining the total differential inductance to meet the voltage droop and return loss specification. A 350uH isolation transformer could be used, but it would have required larger inductors.

    The isolation transformer, T2 in EVAL-ADIN2111D1Z doesn't have a center tap, while T1 in EVAL-ADIN2111EBZ does. C98, R82, C103 provide common-mode termination through the center tap.

    Regarding performance, both the evaluation board designs ensure compliance with the10BASE-T1L standard. The difference in components does not degrade the performance.  

    As for the best solution, it depends on the application requirements. If power forwarding or port to port data bypass is needed, the EVAL-ADIN2111D1Z is the better choice as it is specifically designed to support this feature. 

    Regards,

    Shazia

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.