Hi,
There are some Evaluation Boards from TDK (EVB-DLA-00x) for PoDL which are designed to be used with EVAL-ADIN1100EBZ and EVAL-ADIN1110EBZ.
First Question:
There is a list of components which are used depending of the Power Class.
The only component that changes for each Class is the Differential-mode Choke Power Inductor (DMC), but shouldn't we also change the Common-Mode Choke (CMC)?
In this case the used CMC (RCM70CGI-471) has a Ir = 700mA, how it can withstand the higher Classes currents?

Second Question:
The previous version of TDKs document (Product Brief 2024) didn't have the resistors in parallel in the CMC nor the capacitors. The new version (Product Brief 2025) do have them. Why are they needed?

Thank you,
Edit Notes
The CMC is the RCM70CGI-471 and not the ICI70CGI-222[edited by: inagore at 1:18 PM (GMT -4) on 10 Mar 2025]