Post Go back to editing

10BASET1L, EVAL-ADIN1100EBZ, Power over Data Line (PoDL)

Category: Hardware

Hi,

There are some Evaluation Boards from TDK (EVB-DLA-00x) for PoDL which are designed to be used with EVAL-ADIN1100EBZ and EVAL-ADIN1110EBZ.

First Question:

There is a list of components which are used depending of the Power Class.
The only component that changes for each Class is the Differential-mode Choke Power Inductor (DMC), but shouldn't we also change the Common-Mode Choke (CMC)?
In this case the used CMC (RCM70CGI-471) has a Ir = 700mA, how it can withstand the higher Classes currents?

Second Question:

The previous version of TDKs document (Product Brief 2024) didn't have the resistors in parallel in the CMC nor the capacitors. The new version (Product Brief 2025) do have them. Why are they needed?

Thank you,

Edit Notes

The CMC is the RCM70CGI-471 and not the ICI70CGI-222
[edited by: inagore at 1:18 PM (GMT -4) on 10 Mar 2025]
Parents
  • Hi, 

    I have found that there is nothing wrong.

    For Class 15 (Current ~= 1.5A) the CMC is located after the DMC so the current is not going through the CMC (You don't need to meet the current).

    For other Classes (Class 10 to Class 14 < 700mA) the CMC is located just before the DMC and then the current is passing through it. (In these cases there is no problem because the CMC is 700mA rated and all these classes are rated less current).

    Thank you,

Reply
  • Hi, 

    I have found that there is nothing wrong.

    For Class 15 (Current ~= 1.5A) the CMC is located after the DMC so the current is not going through the CMC (You don't need to meet the current).

    For other Classes (Class 10 to Class 14 < 700mA) the CMC is located just before the DMC and then the current is passing through it. (In these cases there is no problem because the CMC is 700mA rated and all these classes are rated less current).

    Thank you,

Children
  • Hi  

    Thank you for reaching out.

    1. Yes, that' correct. When the CMC is placed before the DMC, then the CMC must be rated to withstand the current, as the current will flow through it. When it's placed after the DMC, this requirement doesn't apply.

     2. The resistors R3 and R4 in parallel with the CMC are to avoid any possible self resonance. Removing them would probably be ok. R5 and R6 are draining resistors for C1 and C2. You could remove them, but they are recommended for draining.

    Regards,

    Shazia