KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADIN2111
Recommended for New Designs
The ADIN2111 is a low power, 2-port 10BASE-T1L transceiver designed for industrial Ethernet applications, and is compliant with the IEEE® 802.3cg-2019â...
Datasheet
ADIN2111 on Analog.com
When power is supplied to ADIN2111 without media connection, a specific pattern seems to be output as shown in the picture below.

However, only one of the two ports outputs and the other does not.
I made 6EA test boards referring to the EVAL-ADIN2111 board..
2EA: 2-port output confirmed
4EA: Only one port output confirmed
The DIP switch settings are the same for all 6EA.
Why does this happen?
SMohammadi - Moved from Other Products (EN) to Physical Layer Devices. Post date updated from Friday, February 28, 2025 6:13 AM UTC to Tuesday, March 11, 2025 4:41 PM UTC to reflect the move.
SMohammadi - Moved from Other Products (EN) to Physical Layer Devices. Post date updated from Tuesday, March 11, 2025 4:41 PM UTC to Tuesday, March 11, 2025 4:41 PM UTC to reflect the move.
Hi cweom
What you're seeing are the autonegotiation signals. These signals should be present on both ports unless the port is in software power down (SWPD) mode or there is potential damage to the boards.
Can you confirm whether the SWPD dip switch is set to not be in SWPD mode?
Regards,
Shazia
I checked the SWPD dip switch and the mode is set.
However, while debugging, I think the cause came from a strange place.
When I measured the waveform directly at pins 4 and 5 of ADIN2111, there was a DC level, but there was no swing of the auto-negotiation signal.
However, when I removed 74930000 and bypassed it, the auto-negotiation signal was measured at pins 4 and 5.
It's strange that the output waveform of ADIN2111 is not measured due to the transformer.
If the PCB I made myself had the same problem, I would suspect the circuit or layout, but the problems are different for each.
Is there any related data on the influence of the transformer and ADIN2111?
Hi cweom
Thank you for sharing your schematic.
It may be that during the assembly of the board, the pads of the transformer were not soldered correctly. We have seen this happen before. Could you please check the solder joints on the transformer pads and ensure they are properly connected?
Regards,
Shazia
Hi cweom
Thank you for sharing your schematic.
It may be that during the assembly of the board, the pads of the transformer were not soldered correctly. We have seen this happen before. Could you please check the solder joints on the transformer pads and ensure they are properly connected?
Regards,
Shazia