Post Go back to editing

What if there is no idle pattern output from ADIN2111?

Category: Hardware
Product Number: ADIN2111

When power is supplied to ADIN2111 without media connection, a specific pattern seems to be output as shown in the picture below.


However, only one of the two ports outputs and the other does not.

I made 6EA test boards referring to the EVAL-ADIN2111 board..

2EA: 2-port output confirmed

4EA: Only one port output confirmed

The DIP switch settings are the same for all 6EA.

Why does this happen?

Thread Notes

Parents Reply Children
  • I checked the SWPD dip switch and the mode is set.


    However, while debugging, I think the cause came from a strange place.

    When I measured the waveform directly at pins 4 and 5 of ADIN2111, there was a DC level, but there was no swing of the auto-negotiation signal.

    However, when I removed 74930000 and bypassed it, the auto-negotiation signal was measured at pins 4 and 5.

    It's strange that the output waveform of ADIN2111 is not measured due to the transformer.

    If the PCB I made myself had the same problem, I would suspect the circuit or layout, but the problems are different for each.

     Is there any related data on the influence of the transformer and ADIN2111?

  • Hi  

    Thank you for sharing your schematic.

    It may be that during the assembly of the board, the pads of the transformer were not soldered correctly. We have seen this happen before. Could you please check the solder joints on the transformer pads and ensure they are properly connected?

    Regards,

    Shazia