Hello,
As you can see in the attached photo, I have connected the 3rd and 4th pair of RJ45 to MDI0 and MDI1 in a setup which should be working with a speed of 100Mbs while the first 2 pairs are connected to MDI2, MDI3 and they are not used. The setup unfortunately doesn't work, I have seen by the data sheet that there's the ability to flip the MDI settings in order to use MDI2 and MDI3 instead of MDI0 and MDI1 via GE_PHY_BASE_CFG register, I have used it but also didn't work although from my point of view it should be working since input at the first 2 pairs of RJ45 to MDI0 and MDI1 has worked in a previous design of us, have you any idea what could be the problem ?