Post Go back to editing

Is it possible to share EFT data with ADIN1200

Category: Datasheet/Specs
Product Number: ADIN1200

Hi 

Is it possible to share "IEC 61000-4-5 surge (±4 kV)" and "IEC 61000-4-4 electrical fast transient (EFT) (±4 kV)" data?

I could find ADIN1300 data below url. but I couldn't find ADIN1200 data.

https://wiki.analog.com/resources/eval/user-guides/adin1300-and-adin1200/cap-coupling

Best regards

Parents Reply
  • Hi,

    Thank you for pointing out this correction in the ADIN1200 datasheet relating to the HX1260NL section. This transformer that is mentioned, the HX1260NL, is the transformer that is used on the Eval Kit and is the recommended transformer for use with the ADIN1200. The ADIN1200 is an Industrial Ethernet PHY, and we do not have a specific Auto grade transformer to recommend, however, transformers that are compliant with the IEEE802.3 Standard should be compatible with the PHY.

    Best Regards,

    Mark

Children
No Data