Hi
ADIN1300
Recommended for New Designs
The ADIN1300 is a low power, single port, Gigabit Ethernet transceiver with low latency and power consumption specifications primarily designed for industrial...
Datasheet
ADIN1300 on Analog.com
Hi
Hi,
The PHY address cannot be read from the PHY or overwritten via MDIO. The Address is set by the hardware strapping, and the device cannot be communicated with unless the device address is know as this is required in both the Clause 22 and Clause 45 frame formats.
Best regards,
Mark
Hi,
The PHY address cannot be read from the PHY or overwritten via MDIO. The Address is set by the hardware strapping, and the device cannot be communicated with unless the device address is know as this is required in both the Clause 22 and Clause 45 frame formats.
Best regards,
Mark