Hello,
In order to save part number and to avoid design complexity I want to use an ADIN2111 as a controller instead of ADIN1100 to command multiple ADIN2111 that are placed in a daisy-chain configuration.
I imagine to do that by just connecting PORT 2 and making PORT 1 to be open circuit.
I read in datasheet (p.14 ) that it is possible to configure ADIN2111 as „Store and forward (to or from the SPI host)“
(The datasheet P.41) tells us that in Transmission-mode the destination Port (1 or 2) also can be determined by bit D0 inside the Frame Header.
Can you please justify that I’m correct about this fact or not?
Thank you so much for your time and considerations.