Post Go back to editing

ADIN1100 RGMII 2.5 MHz RGMII Transmit Clock Input (TXC) confirmation input or output?

Category: Hardware
Product Number: ADIN1100

HI,

I am working on design using the ADIN1100 , I am connecting into a Ethernet switch via the RGMII port. Looking at the datasheet, pin 38 TXC is stated as the 2.5MHz RGMII Transmit Clock Input which meets requirements BUT in the RGMII Interface Mode section page 14 of the datasheet it implies that the clock is generated as per the the following... "For the RGMII transmit interface, the ADIN1100 generates a 2.5 MHz reference clock on TX_CLK."

Can you please confirm whether the ADIN1100 generates the RGMII TXC clock OR the clock is driven by the switch MAC??

Thanks


 

Parents
  • Hi,

    Thank you for bringing this to our attention. I can confirm the following sentence in Page 14 is a typo:

    "For the RGMII transmit interface, the ADIN1100 generates a 2.5 MHz reference clock on TX_CLK"

    It should say:

    "For the RGMII transmit interface, the MAC generates a 2.5 MHz reference clock on TXC".

    The TXC clock is driven by the switch MAC. We take note to correct this in a future revision of the data sheet.

    Regards,

    Raquel.

Reply
  • Hi,

    Thank you for bringing this to our attention. I can confirm the following sentence in Page 14 is a typo:

    "For the RGMII transmit interface, the ADIN1100 generates a 2.5 MHz reference clock on TX_CLK"

    It should say:

    "For the RGMII transmit interface, the MAC generates a 2.5 MHz reference clock on TXC".

    The TXC clock is driven by the switch MAC. We take note to correct this in a future revision of the data sheet.

    Regards,

    Raquel.

Children
No Data