Post Go back to editing

when the ADIN1200 is powered off

Category: Datasheet/Specs
Product Number: ADIN1200

When the device in which the ADIN1200 is installed is turned off, that is, when the ADIN1200 is powered off,

I think that there is a state in which voltage is applied to the MDI_x_x terminals from other powered devices via cables and pulse transformers.

Q1 In the above state, it is thought that the maximum absolute rating of the MDI_x_x terminal ~ AVDD_3P3 + 0.3V will be exceeded, but is it NG?

Q2 If you have any advice on countermeasures, please let me know