Post Go back to editing

ADIN 1110 None-OS driver

Category: Software
Product Number: EVAL-ADIN1110EBZ 08-064213 REV B
Software Version: NUCLEO L4R5ZI (host MCU)

Hello Ladies and Gentlemen,

I am testing None-OS Driver for µC extern L4R5ZI. I use HardwareLoopback as an example. The functionality of the interfaces like SPI, reset pin and INT_N are tested before adding the driver. Now there is a problem with "MAC_Init" and it is in the location "MAC_Reset". It is not correctly returning from the function here. Do you have any suggestions or we can fix this error. Because of this error HardFault interrupt is fired.

the µC on the EVAL board is in reset state.

Thank you so much 

STM32Cube IDE 

Spi generic 

Without CRC 

USE_NUCLEO 

USE_HAL_DRIVER 

Top Replies

    •  Analog Employees 
    May 19, 2022 in reply to stmoabba +2 verified

    Hi  ,

    Great that you have it working.

    Just for completeness, as discussed separately the issue was related to the SPI CRC configuration defined by the hardware strapping pin SPI_CFG0 (CRC/OA protection…

    •  Analog Employees 
    May 19, 2022 in reply to stmoabba +1 verified

    Hi  ,

    We provided you with another board with the silicon revision 2 that supports the Open Alliance protocol.

    • Can you send a picture of your setup?
    • Can you provide a schematics description of…