Hello,
I'm trying to set up a ADIN1300, but i don't get i working. Now I found some behavior I don't understand. I activated the linedriver loopback mode and sending out a ping. I can measure the TXC and also signals on the Data lines. The clock has a frequency of 125MHz, as I expected a 1000Mb/s. But the RXC only has a frequency of 62.5MHz and the Mac does not receive any packages.
If i switch to 100Mb/s speed, TXC goes to 25MHz and RXC to 12.5MHz.
Any idea what is going wrong here? The ADIN1300 is interfaced via RGMII, the clock is supplied by a HCMOS oscillator with 25MHz, 1.8V square wave.
Greetings
Julian
[locked by: CatherineR at 3:47 PM (GMT -5) on 23 Nov 2021]
[unlocked by: CatherineR at 3:48 PM (GMT -5) on 23 Nov 2021]
[locked by: CatherineR at 2:32 PM (GMT -5) on 13 Dec 2021]